Part Number: DP83TC811S-Q1
Other Parts Discussed in Thread: DP83TC811
HI TEAMS:
We are debugging the sleep wake function of dp83tc811 chip
I found I couldn't sleep.
Condition: pull up the wake before the PHY is powered on, and the PHY chip can be recognized normally. It is only set to the slave mode and is not connected to the device in the master mode.

Set according to figure 1:
1. Lower the wake foot
2. Set register 0x18b to 0x5b, register 0x4e5 to 0x3c3, register 0x487 to 0xa01 and register 0x18c to 0x2
Check that the INH pin does not go high, indicating that it has not entered sleep.
We found that our phenomenon is the same as that of the forum, e2e.ti.com/.../2729720 -sitesearch&keymatch=dp83tc811%252525252525252520sleep#2729720

So we measured the level of MDIO and kept it at the high level. Is it because of the high level that we cannot sleep?