Hello,
One customer met a question about GPIO0 pass though and I2S_WC conflict when used DS90UB947+DS90UB948. The phenomenon is as following:
1. If DS90UB947 0x12=0x2, GPIO0 pass through failed. But the I2S_DA ,CLK,WC of DS90UB948 output normally and sound is also normal. 948: 0x28=0x10
2. If 947:0x12=0x0, 0x4=0x90,GPIO0 pass though successfully. But I2S_DA ,CLK of DS90UB948 output normally, while I2S_WC output abnormally, the WC output frequency isn't sample rate, the sound also is
abnormal. Please refer to the waveform of I2S_WC( Above is input, we can see the output of the below is changed the sample rate)
3. One question is confused is that if 0x54 bit0=1 of DS90UB947( datasheet described this bit is Reserved), GPIO0 pass through failed, 0x12=0x0 also pass through failed. 0x28 of DS90UB948 is 0x10.


Best regard
Kailyn