This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI recommendation

Hello:

Please help recommend suitable TI chip,below is requirement,Thanks!!!

1、SDIO to Ethernet control chip: support 100M Ethernet

2、USB to Ethernet control chip, only two EP

3、SPI to USB host chip: 24mbps

  • Hi Jimmy,

    Thank you for getting in touch with us.

    We don't have a standalone SDIO to Ethernet control analog device. However, AM355x family probably supports all of the above. You just have to use one of the AM355x devices (for SDIO to MII conversion) and club them with ethernet standalone PHY (MII to Copper).

    I am not an expert in AM355x processors and USB devices. I can put you in touch with one of the experts in that product line.
    Please let me know if you are okay with it.

    --
    Regards,
    Gokul.