I required a suitable part from TI for the below requirement.
- Coming from the ADAS it shifts the data back to us in an LVDS stream. We will convert the LVDS to a single ended 0-1.8V CMOSing ( LVDS to CMOS to TTL convertor chip. It could go into a port in the imx8. It will need to go to some other synchronous series port. One mx8 will be just convert the data and place it in the memory.
It is for a medical application.
Earlier we have used Intel cyclone10 FPGA between the ADAS1135 and IMX8MQ processor, due to supply chain issue we are planning to remove FPGA and adding LVDS to CMOS to TTL converter chip.
Please suggest the part which can fulfil my requirement.
Regards,
Jyothi.