Part Number: DS80PCI402
We are having issues with PCIe communication on a DS80PCI402, driving a VPX card on one side and two in series 1M iPASS cables on the other side. Does this device support any type of S/W app/circuit that allows the received eye to be observed via at the redriver device via its I2C bus? Any recommendations for resolving other than soldering scope leads to the DS80PCI402 device pins and monitoring the eye via scope/diff probe? The pitch of the redriver package doesn’t lend itself to easily monitor the signals at this point.
Links are Gen 2, 5G, but connect at either 2.5G or not at all.