Other Parts Discussed in Thread: DP83TC811
I have a question.
Currently, when the PHY kernel driver of DP83TC811 is activated, it is recognized as 10Mbps/half and works
I'm not doing it.
So, without using the PHY kernel driver of DP83TC811, I will force the setting as below
It is confirmed that there is no problem with the default behavior and hw.
As a result, there is a problem that the mdio communication is not working and the phy status cannot be checked frequently.
• uboot settings
Add to uboot/configs/en675_defconfig
CONFIG_PHY_FIXED=y
at uboot/arch/riscv/dts/eyenix_en675.dts
Locate the ETH and add its fixed-linx portion
ETH {
....
fixed-link {
speed = <100>;
full-duplex;
};
};
• linux settings
Add to conf/linux/defconfig_all
CONFIG_FIXED_PHY=y
Add full to the bottom of conf/en675X/en675X_device_tree.dts
Ð {
fixed-link {
speed = <100>;
full-duplex;
};
};
Therefore, since mdio communication is required, I will activate the PHY kernel driver and skip the // part below
ethtool -seth0 speed 100 duplex full autoneg off processing
1) Modify dp83811_config_init function in linux/drivers/net/py/dp83tc811.c (note 5,6,7 lines)
1. static int dp83811_config_init(struct phy_device *phydev)
2. {
3. int value, err;
4.
5. // err = genphy_config_init(phydev);
6. // if (err < 0)
7. // return err;
8.
9. value = phy_read(phydev, MII_DP83811_SGMII_CTRL);
if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
2) Execute the command below when it is subsequently booted
ethtool -s eth0 speed 100 duplex full autoneg off
In the case of number 2, it is possible to check the phy status through mdio as well as network communication.
// SPDX-License-Identifier: GPL-2.0
/*
* Driver for the Texas Instruments DP83TC811 PHY
*
* Copyright (C) 2018 Texas Instruments Incorporated - http://www.ti.com/
*
*/
#include <linux/ethtool.h>
#include <linux/etherdevice.h>
#include <linux/kernel.h>
#include <linux/mii.h>
#include <linux/module.h>
#include <linux/of.h>
#include <linux/phy.h>
#include <linux/netdevice.h>
#define DP83TC811_PHY_ID 0x2000a253
#define DP83811_DEVADDR 0x1f
#define MII_DP83811_SGMII_CTRL 0x09
#define MII_DP83811_INT_STAT1 0x12
#define MII_DP83811_INT_STAT2 0x13
#define MII_DP83811_INT_STAT3 0x18
#define MII_DP83811_RESET_CTRL 0x1f
#define DP83811_HW_RESET BIT(15)
#define DP83811_SW_RESET BIT(14)
/* INT_STAT1 bits */
#define DP83811_RX_ERR_HF_INT_EN BIT(0)
#define DP83811_MS_TRAINING_INT_EN BIT(1)
#define DP83811_ANEG_COMPLETE_INT_EN BIT(2)
#define DP83811_ESD_EVENT_INT_EN BIT(3)
#define DP83811_WOL_INT_EN BIT(4)
#define DP83811_LINK_STAT_INT_EN BIT(5)
#define DP83811_ENERGY_DET_INT_EN BIT(6)
#define DP83811_LINK_QUAL_INT_EN BIT(7)
/* INT_STAT2 bits */
#define DP83811_JABBER_DET_INT_EN BIT(0)
#define DP83811_POLARITY_INT_EN BIT(1)
#define DP83811_SLEEP_MODE_INT_EN BIT(2)
#define DP83811_OVERTEMP_INT_EN BIT(3)
#define DP83811_OVERVOLTAGE_INT_EN BIT(6)
#define DP83811_UNDERVOLTAGE_INT_EN BIT(7)
/* INT_STAT3 bits */
#define DP83811_LPS_INT_EN BIT(0)
#define DP83811_NO_FRAME_INT_EN BIT(3)
#define DP83811_POR_DONE_INT_EN BIT(4)
#define MII_DP83811_RXSOP1 0x04a5
#define MII_DP83811_RXSOP2 0x04a6
#define MII_DP83811_RXSOP3 0x04a7
/* WoL Registers */
#define MII_DP83811_WOL_CFG 0x04a0
#define MII_DP83811_WOL_STAT 0x04a1
#define MII_DP83811_WOL_DA1 0x04a2
#define MII_DP83811_WOL_DA2 0x04a3
#define MII_DP83811_WOL_DA3 0x04a4
/* WoL bits */
#define DP83811_WOL_MAGIC_EN BIT(0)
#define DP83811_WOL_SECURE_ON BIT(5)
#define DP83811_WOL_EN BIT(7)
#define DP83811_WOL_INDICATION_SEL BIT(8)
#define DP83811_WOL_CLR_INDICATION BIT(11)
/* SGMII CTRL bits */
#define DP83811_TDR_AUTO BIT(8)
#define DP83811_SGMII_EN BIT(12)
#define DP83811_SGMII_AUTO_NEG_EN BIT(13)
#define DP83811_SGMII_TX_ERR_DIS BIT(14)
#define DP83811_SGMII_SOFT_RESET BIT(15)
static int dp83811_ack_interrupt(struct phy_device *phydev)
{
int err;
err = phy_read(phydev, MII_DP83811_INT_STAT1);
if (err < 0)
return err;
err = phy_read(phydev, MII_DP83811_INT_STAT2);
if (err < 0)
return err;
err = phy_read(phydev, MII_DP83811_INT_STAT3);
if (err < 0)
return err;
return 0;
}
static int dp83811_set_wol(struct phy_device *phydev,
struct ethtool_wolinfo *wol)
{
struct net_device *ndev = phydev->attached_dev;
const u8 *mac;
u16 value;
if (wol->wolopts & (WAKE_MAGIC | WAKE_MAGICSECURE)) {
mac = (const u8 *)ndev->dev_addr;
if (!is_valid_ether_addr(mac))
return -EINVAL;
/* MAC addresses start with byte 5, but stored in mac[0].
* 811 PHYs store bytes 4|5, 2|3, 0|1
*/
phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_DA1,
(mac[1] << 8) | mac[0]);
phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_DA2,
(mac[3] << 8) | mac[2]);
phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_DA3,
(mac[5] << 8) | mac[4]);
value = phy_read_mmd(phydev, DP83811_DEVADDR,
MII_DP83811_WOL_CFG);
if (wol->wolopts & WAKE_MAGIC)
value |= DP83811_WOL_MAGIC_EN;
else
value &= ~DP83811_WOL_MAGIC_EN;
if (wol->wolopts & WAKE_MAGICSECURE) {
phy_write_mmd(phydev, DP83811_DEVADDR,
MII_DP83811_RXSOP1,
(wol->sopass[1] << 8) | wol->sopass[0]);
phy_write_mmd(phydev, DP83811_DEVADDR,
MII_DP83811_RXSOP2,
(wol->sopass[3] << 8) | wol->sopass[2]);
phy_write_mmd(phydev, DP83811_DEVADDR,
MII_DP83811_RXSOP3,
(wol->sopass[5] << 8) | wol->sopass[4]);
value |= DP83811_WOL_SECURE_ON;
} else {
value &= ~DP83811_WOL_SECURE_ON;
}
value |= (DP83811_WOL_EN | DP83811_WOL_INDICATION_SEL |
DP83811_WOL_CLR_INDICATION);
phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG,
value);
} else {
value = phy_read_mmd(phydev, DP83811_DEVADDR,
MII_DP83811_WOL_CFG);
value &= ~DP83811_WOL_EN;
phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG,
value);
}
return 0;
}
static void dp83811_get_wol(struct phy_device *phydev,
struct ethtool_wolinfo *wol)
{
u16 sopass_val;
int value;
wol->supported = (WAKE_MAGIC | WAKE_MAGICSECURE);
wol->wolopts = 0;
value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG);
if (value & DP83811_WOL_MAGIC_EN)
wol->wolopts |= WAKE_MAGIC;
if (value & DP83811_WOL_SECURE_ON) {
sopass_val = phy_read_mmd(phydev, DP83811_DEVADDR,
MII_DP83811_RXSOP1);
wol->sopass[0] = (sopass_val & 0xff);
wol->sopass[1] = (sopass_val >> 8);
sopass_val = phy_read_mmd(phydev, DP83811_DEVADDR,
MII_DP83811_RXSOP2);
wol->sopass[2] = (sopass_val & 0xff);
wol->sopass[3] = (sopass_val >> 8);
sopass_val = phy_read_mmd(phydev, DP83811_DEVADDR,
MII_DP83811_RXSOP3);
wol->sopass[4] = (sopass_val & 0xff);
wol->sopass[5] = (sopass_val >> 8);
wol->wolopts |= WAKE_MAGICSECURE;
}
/* WoL is not enabled so set wolopts to 0 */
if (!(value & DP83811_WOL_EN))
wol->wolopts = 0;
}
static int dp83811_config_intr(struct phy_device *phydev)
{
int misr_status, err;
if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
misr_status = phy_read(phydev, MII_DP83811_INT_STAT1);
if (misr_status < 0)
return misr_status;
misr_status |= (DP83811_RX_ERR_HF_INT_EN |
DP83811_MS_TRAINING_INT_EN |
DP83811_ANEG_COMPLETE_INT_EN |
DP83811_ESD_EVENT_INT_EN |
DP83811_WOL_INT_EN |
DP83811_LINK_STAT_INT_EN |
DP83811_ENERGY_DET_INT_EN |
DP83811_LINK_QUAL_INT_EN);
err = phy_write(phydev, MII_DP83811_INT_STAT1, misr_status);
if (err < 0)
return err;
misr_status = phy_read(phydev, MII_DP83811_INT_STAT2);
if (misr_status < 0)
return misr_status;
misr_status |= (DP83811_JABBER_DET_INT_EN |
DP83811_POLARITY_INT_EN |
DP83811_SLEEP_MODE_INT_EN |
DP83811_OVERTEMP_INT_EN |
DP83811_OVERVOLTAGE_INT_EN |
DP83811_UNDERVOLTAGE_INT_EN);
err = phy_write(phydev, MII_DP83811_INT_STAT2, misr_status);
if (err < 0)
return err;
misr_status = phy_read(phydev, MII_DP83811_INT_STAT3);
if (misr_status < 0)
return misr_status;
misr_status |= (DP83811_LPS_INT_EN |
DP83811_NO_FRAME_INT_EN |
DP83811_POR_DONE_INT_EN);
err = phy_write(phydev, MII_DP83811_INT_STAT3, misr_status);
} else {
err = phy_write(phydev, MII_DP83811_INT_STAT1, 0);
if (err < 0)
return err;
err = phy_write(phydev, MII_DP83811_INT_STAT2, 0);
if (err < 0)
return err;
err = phy_write(phydev, MII_DP83811_INT_STAT3, 0);
}
return err;
}
static int dp83811_config_aneg(struct phy_device *phydev)
{
int value, err;
if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
value = phy_read(phydev, MII_DP83811_SGMII_CTRL);
if (phydev->autoneg == AUTONEG_ENABLE) {
err = phy_write(phydev, MII_DP83811_SGMII_CTRL,
(DP83811_SGMII_AUTO_NEG_EN | value));
if (err < 0)
return err;
} else {
err = phy_write(phydev, MII_DP83811_SGMII_CTRL,
(~DP83811_SGMII_AUTO_NEG_EN & value));
if (err < 0)
return err;
}
}
return genphy_config_aneg(phydev);
}
static int dp83811_config_init(struct phy_device *phydev)
{
int value, err;
err = genphy_config_init(phydev);
if (err < 0)
return err;
value = phy_read(phydev, MII_DP83811_SGMII_CTRL);
if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
err = phy_write(phydev, MII_DP83811_SGMII_CTRL,
(DP83811_SGMII_EN | value));
} else {
err = phy_write(phydev, MII_DP83811_SGMII_CTRL,
(~DP83811_SGMII_EN & value));
}
if (err < 0)
return err;
value = DP83811_WOL_MAGIC_EN | DP83811_WOL_SECURE_ON | DP83811_WOL_EN;
return phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG,
value);
}
static int dp83811_phy_reset(struct phy_device *phydev)
{
int err;
err = phy_write(phydev, MII_DP83811_RESET_CTRL, DP83811_HW_RESET);
if (err < 0)
return err;
return 0;
}
static int dp83811_suspend(struct phy_device *phydev)
{
int value;
value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG);
if (!(value & DP83811_WOL_EN))
genphy_suspend(phydev);
return 0;
}
static int dp83811_resume(struct phy_device *phydev)
{
int value;
genphy_resume(phydev);
value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG);
phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG, value |
DP83811_WOL_CLR_INDICATION);
return 0;
}
static struct phy_driver dp83811_driver[] = {
{
.phy_id = DP83TC811_PHY_ID,
.phy_id_mask = 0xfffffff0,
.name = "TI DP83TC811",
.features = PHY_BASIC_FEATURES,
.flags = PHY_HAS_INTERRUPT,
.config_init = dp83811_config_init,
.config_aneg = dp83811_config_aneg,
.soft_reset = dp83811_phy_reset,
.get_wol = dp83811_get_wol,
.set_wol = dp83811_set_wol,
.ack_interrupt = dp83811_ack_interrupt,
.config_intr = dp83811_config_intr,
.suspend = dp83811_suspend,
.resume = dp83811_resume,
},
};
module_phy_driver(dp83811_driver);
static struct mdio_device_id __maybe_unused dp83811_tbl[] = {
{ DP83TC811_PHY_ID, 0xfffffff0 },
{ },
};
MODULE_DEVICE_TABLE(mdio, dp83811_tbl);
MODULE_DESCRIPTION("Texas Instruments DP83TC811 PHY driver");
MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com");
MODULE_LICENSE("GPL");
Please help me with what I can do to solve the problem.