Part Number: TDP142
Hi Team,
Please advice me ony two questions bellows.
Q1 The datasheet insits that Pin11 (A0) "When I2C_EN = 0, leave the pin unconnected. "
On the otherhand, the refrence schematic recomends that this pin is connected to
GND through the 1 ko ohm resister.
Can this pin conned to GND through GND when the device is configured in GPIO mode?
Q2. I suspect that DP specifications recomed DP conector pin 13 and 14 (Config1 and Config2)
are connected to GND through 1 Meg ohm resisters respectivly.
However, the refrence schematic recomends that pin 14 is connected to GND through a
5 Meg ohm resister instead of 1 Meg ohm one.
Is the 5 Meg ohm correct value?
Mita