Part Number: TUSB4041I
Hi,
Test TUSB4041IPAP USB HUB function no, test power 3.3V and 1.1V no problem, reset signal is good, external hung to an EEPROM, no program at that time, 24MHZ clock output abnormal.File a schematic for this section
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB4041I
Hi,
Test TUSB4041IPAP USB HUB function no, test power 3.3V and 1.1V no problem, reset signal is good, external hung to an EEPROM, no program at that time, 24MHZ clock output abnormal.File a schematic for this section
Thanks!
Hi,
The crystal will stop when the hub is suspended or not connected to a host.
If a host is connected to the hub, but there are no downstream devices connected the host will often suspend the hub.
Are the hub / downstream device enumerating correctly or not?
Can you send a clock waveform? Does the waveform improve if you replace the 33ohm resistor with 0ohm and change the crystal loading capacitor.
Thanks
David
Hi David,
Today we did a few tests:
1. At present, we will fly the uplink USB2.0 interface out, and the mouse connection is OK.
2, clock 24MHZ is the drawing of FB14 welding, and then output.
3. 1pcs EEPROM is externally connected on the drawing, the model is at24c04bn-sh. Does this EEPROM need burning program?
4. The power supply has been adjusted according to the chip data, 3.3V>>1.1V
5. At present, some IO status errors are suspected, please help to check the schematic diagram
Thank you very much!
Hi,
Is SMBUSz being pulled high or low? if the TUSB4041 has SDA/SCL pulled high and a blank EEPROM attached, it will automatically enter programming mode and stay there until the EEPROM is programmed. While in programming mode, the hub will not function as a hub.
You can leave SMBUSz as NC if external interface is not required.
Looking at the schematic, you do not need the common mode choke on the hub upstream port.
Thanks
David
Hi David,
I try to leave SMBUSz as NC, but the HUB is also not work. Now the EEPROM is a blank EEPROM.
Does the hub chip need firmware when it works?Can you send a firmware? Let's burn it to EEPROM to try.
the common mode choke on the hub upstream port, I don't think it will cause this hub to not work,So I didn't delete it.
Thanks.
Hi,
The EEPROM is optional, the hub will work without the EEPROM.
In your earlier message, you said the mouse connection is ok, so it looks like the hub is correctly being enumerated, is this correct?
Can you please send a picture of the clock waveform and have you tried to change the 33ohm to 0ohm on the crystal input and output?
Thanks
David
Hi David,
1. I'm sorry, maybe I didn't make it clear. Currently, I can't connect the mouse either. I've been synchronising the test and the waveform will be sent out.At the moment it has a waveform at 33 ohm.
2. Whether EEPROM needs driver, as I have seen doing this related post, https://e2e.ti.com/support/interface-group/interface/f/interface-forum/622318/tusb4041papevm-were-can-i-get-the-microsoft-windows-based-eeprom-utility-and-windows-drivers-for-the-tusb4041-eeprom-programming-interface-with-vid-0451-and-pid-80ff
3. Is there any documentation about TUSB4041 design and debugging steps?
Many thanks!
Hi,
1. SMBUS/I2C is not required is only needed if you want to change the default configuration of the hub. It is also important to not leave blank EEPROMs connected to the hub if not used, the hub will enter a programming mode.
2. For debugging, please refer to this e2e FAQ, https://e2e.ti.com/support/interface-group/interface/f/interface-forum/719918/faq-how-do-i-debug-a-ti-usb-hubs-when-downstream-ports-are-non-operational. But it is important that the clock must oscillate first.
Thanks
David
Hi,
Awesome. Thanks for the update and I am glad you are able to solve the issue. Any chance you can share the root cause of the issue?
Wish you a Happy Mid-Autumn Festive as well!
David
Hi David,
1. There is a problem with the common mode inductor of the uplink connection of the HUB, which leads to the failure of connecting the uplink port and the USB hub.
2.EEPROM really needs to be removed, otherwise it will default to wait to burn node.
Hi,
Thanks for the detailed explanation. Again, I am glad you are able to solve your issue.
David