This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2N2222



We are seeing an issue where we are seeing failures in a current measurement test for a transistor and Op Amp circuit that are temperature related.  We see no failures at low temperatures.  As the temperature rises failures begin to occur at about 116 F and continue to increase until we reach a temperature range of just over 130 F where the temperature levels off and failure occurrences drastically reduce.  Are temperature changes typically cause more failures than a constant higher temperature that is still within the defined range of operating temperatures for the part?  We suspect the part that has the failures is a 2N2222.  Do you make heat sinks for that part?  The real issue is a 5 VDC power supply that is mounted to a heat sink plate close to the transistor.  The power supply becomes very hot. We are looking at various options to correct this one is to add a heat sink to the transistor.  Thank you for any advice you can provide.

  • Hello Glenn,

      The 2N2222 BJT is not a TI device, therefore, we cannot comment on your inquiry. 

    You will have to find a semiconductor company that produces the 2N2222 for technical assistance. 

    Regards, 

    ~Leonard  

  • I wasn't necessarily referring to the 2N2222 specifically. My question is in general how does change in temperature compare to a steady state high temperature.  Which case is more likely to cause a failure in a transistor or logic device?  A 2N2222 just happened to be a part we use.  It is now obsolete.  It was originally designed by Motorola in the 60s but when I looked up manufacturers TI was listed as one.  I guess that was incorrect.  Thanks for the reply.

  • All electrical components have temperature-dependent characteristics (which are usually shown in the datasheet). It is the duty of the circut designer to ensure that those do not result in failures.

    I cannot say anything specific because I do not know your circuit, or what particular behaviour you consider a failure. If you'd show a schematic with a TI opamp, your question would be on topic here.