Part Number: DS250DF230
Hi,
The customer wants to combine an MSP430F5419AIPZR (master) with a DS250DF230ZLSR (slave) for I2C communication.
From the thread below, we can read Clock low period (min) = 1.3 us (400kHz class).
1. Is the DS250DF230 ”clock low period" rounded up to 1.3us?
2. Can they use the DS250DF230 "clock low period" at 1.28us?
3. Is there a timing chart with tlow, tSU_DAT, etc.?
Best Regards,
Nishie