Part Number: TCA9548A
There are mainly two questions that need your help to confirm:
1. As an extended I2C chip, if the address of tca9548pwr is set to 0x70 (or other fixed address), can the address of I2C device mounted on the extended 8-channel I2C bus not be 0x70?
2. Since the PCB has been proofed, at present, tca9548pwr A0, A1 and A2 are grounded, and the address is 0x70, there will be address conflict in application.
The PCB is connected as follows: A0 and A1 are short circuited with reset and pulled up to 3.3V through a 10kohm resistor, A2 is connected to GND, and the address changes to 0x73. Is it OK?