Part Number: TS3USB221
Other Parts Discussed in Thread: TMUXHS221
Hi team,
May I know what has improve or different from TS3USB221 to TMUXHS221 ,
please send me the comparison table if it's OK, thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMUXHS221 is P2P to some competitor's device, it also have higher bandwidth.
Hi Brian,
I don't get it.
USB 2.0 bandwidth doesn't change at all (480Mbps), why would bandwidth be higher?
Can you elaborate the difference ? like insertion loss?
BW is the frequency where 3db insertion loss is.
Some customers may need to switch between USB2 and some other signals need a little higher BW, 1Ghz or 2Ghz.
Regards
Brian
Hi Brian,
take I3C for example , I think both device can support I3C right?
i3C is only 12.5MHZ lower than type-C SBU frequency
and would you let me know when is the RTM date of TMUXHS221? email would be fine a well
thanks
yes, it should work.
RTM is around end of Dec, but you can order sample now.
Thanks
Brian