This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ONET1130EP: Suitable for DML application?

Expert 5170 points

Part Number: ONET1130EP

Dear e2e support,

Could you confirm if the ONET1130EP part could be used in DML application (vs EML as mentioned in the datasheet)?

What would be the limitation?

Regards,

  • Greetings,

    EML parts topically have high single ended output swing into 50 ohm loaded. These are typically used for long haul lasers. On the other hand DML driver are mainly current modulators and typically deliver up to 85mA into 25-30 ohm load for enterprise or medium distance. So the applications are different and it all depends on your laser specification/application or laser being used.

    Regards,Nasser