Part Number: DP83867IR
Hi team,
DP83867IR doesn’t link up correctly with certain systems with the 100BASE full duplex fixed mode which registers are set below:
- Address 0x0009:0x0000
1000BASE-T Full/Half set to OFF - Address 0x0012:0x6400
Interrupt setting
- Address 0x0000:0x2100
100Mbps fixed, auto negotiation set to OFF - Address 0x0086:0x0073
TX/RX delay setting - Address 0x0018:0x6B50
LED2 setting - Address 0x012C:0x0E81
datasheet recommendation to improve the short cable performance
Could you help me to address this issue?
Note: #1 and #3 are the specific settings for 100BASE full duplex fixed mode.
When AUTO-NEGOTIATION mode, it works correctly.
Regards,
Itoh