Part Number: SN75LVDS84A
Other Parts Discussed in Thread: DS90C363B,
Hi,
Due to semicondutor shortage, I had no options to buy the current RBG->LVDS transmitter that I use in my project (DS90C363B).
I saw in the documentation the directly substitute for this item is the SN75LVDS84A.
We buy the SN75LVDS84A and replace it in two board to test.
After replacement, the image was blurred. The figure below shows the effect.
https://drive.google.com/file/d/1dXDonz65ia6J9oOjhS794t0J3Whk8OQH/view?usp=sharing

This is the schematic of my project (in my drive to high definition):
https://drive.google.com/file/d/1WS5uKoryP8dJHPqnXt-YchGFSI1VgcgL/view?usp=sharing

The CLOCK of the display is 50MHz (Typ.).
We try to remove the R600, left the pin 14 not connect, like the datasheet recommended, but nothing changes.
I appreciate any help with it.
Thanks!