Part Number: THVD1550
Hi Teams,
Here are some questions about THVD1550.
1) from the data sheet it seems if the TX and RX were disabled together, it takes us to enable again. Is correct?
2) If the Re and DE were connect together. Ideally, the system will not enter 'shutdown' mode. But, if the signal delay is too large or slop is not sharp enough, will the system enter 'shutdown' accidently? If so, is the time limit equal to the disable time?

Many thanks.
Br,
Hugh