This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: About Usage for USB PD

Guru 21045 points

Part Number: TUSB4020BI

Hi Team,

 

Our customer would like to connect USB 2.0 HUB(TUSB4020BI) and USB PD adapter to same Type-C connector on board.

So, USB2.0 communication by HUB(device(UP)=>HUB=>device(DOWN)) and power supply(DFP 9V/2A) by USB PD(Adapter=>device) are performed at the same time.

-USB_DP_UP and USB_DM_UP of TUSB4020BI connect to VBUS, D+, D-, GND

-USB PD Adapter connect to VBUS, CC lines

 

Then, can TUSB4020BI communicate properly?

I'm worried about the effects of VBUS voltage changes etc.

 

And, could you please let us know if you have other recommended device?

 

[Image]

 

 

Regards,

Hide