Part Number: DS16EV5110A
Hi,
As recommending the input and output differential pair length match in EVM schematic as shown below, kindly provide length matching details and tolerance for both input and output side.

Regards,
Sreekanth
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS16EV5110A
Hi,
As recommending the input and output differential pair length match in EVM schematic as shown below, kindly provide length matching details and tolerance for both input and output side.

Regards,
Sreekanth
Hi Sreekanth,
The DVI Specification V1.0 specifies that the allowable intra-pair skew at the receiver connector is 0.4 Tbit and the allowable inter-pair skew at receiver connector is 0.6 Tpixel.
For further information on this, please see the DVI specification.
Thanks,
Drew
Hi Sreekanth,
The above is a system specification. The redriver itself does not have an inter-pair skew specification that is required for it to operate properly, but the overall system requires inter-pair skew within 0.6 Tpixel.
Regarding intra-pair skew, the datasheet recommends using the same length traces for differential pairs.

In terms of a tolerance, I would leverage the following resource. However, ideally try to keep the pair as similar in length as possible.
Thanks,
Drew