Part Number: DSLVDS1047
Hi Expert,
Does DSLVDS1047 have internal clamp diode between DIN and Vcc?
I believe this device have diode, because the Abs max of DIN is Vcc+0.3V.
Customer is considering abnormal condition about applying any signal to DIN during Vcc power down.
(They understand, it is not recommended condition because exceed Abs max. )
When they try to test this condition. They cannot see any leakage to Vcc.
So, they would like to confirm about internal clamp diode.
CH1:VCC、CH2~4:DIN1~3

Thanks
Muk