Part Number: DP83TG720EVM-MC
Hi,
I want to use two of the above kits in back to back to back mode to connect between two PCs with RJ45.
So one PC with RG45 is connected to one of the kits. That kit is connected with the other kit using the automotive cable provided in the kit. The second kit is connected to another PC:
PC1 ----> DP83TG720EVM-MC ---------> automotive cable ------> DP83TG720EVM-MC ----------> PC2
I assigned static addresses 192.168.1.1 and 192.168.1.10 to each PC respectively.
Also connected micro USB cable to each kit to provide power - green LEDs turn on in each.
Now if I do a ping from PC1 to PC2 or vice versa, it does not work. Does that mean that above setup is not possible or do I need to do something else also?
Also I see address 192.168.1.2 assigned to some thing as ping to that worked. Is this the address of the kit itself?
Regards
Nadeem