Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: DS90UB934-Q1, , DS90UB933-Q1
HI TEAMS:
In the model selection stage of an existing project, the front end generates mipi dsi or RGB signals( 1280x720@60hz )The rear display screen uses DS90UB934-Q1
, please help determine the intermediate conversion bridging scheme,
1. Please confirm whether DS90UB941 can be used as the intermediate transfer bridge;
2. If the DS90UB941 is not feasible, can you convert dsi -->bt656 -->DS90UB933-Q1
, but if the bt565 is SDR 148Mhz, ask whether the DS90UB933-Q1 supports it;
Please help to confirm, thank you!