Part Number: TUSB8043
Other Parts Discussed in Thread: TUSB8044AEVM
HI All,
We have used USB hub controller (TUSB8043RGCT) in our design. According to the design, we have connected the upstream to Host processor and Down stream(USB 3.0) Port 1 is connected to LTE module and Downstream(USB 3.0) Port 2 is connected to Type C. When we test the LTE module (Port 1), it fails 3 out of 10 times . Thus, we decided to test the LTE module in the below conditions listed as follows:
1. We tested the LTE module in the DEV kit to recreate the issue but we could not see the issue with the LTE module.
2. We also didn’t face any issues when we test the LTE module on another board that does not have a HUB controller where USB 3.0 is directly connected to the host processor.
Could you please help us to find the root cause and resolve the issue?
Below is the failure log for your reference.
[ 333.219668] option1 ttyUSB0: usb_wwan_indat_callback: resubmit read urb failed. (-2)
[ 333.219850] option1 ttyUSB0: usb_wwan_indat_callback: resubmit read urb failed. (-2)
[ 333.220000] option1 ttyUSB0: usb_wwan_indat_callback: resubmit read urb failed. (-2)
[ 333.223300] option1 ttyUSB0: GSM modem (1-port) converter now disconnected from ttyUSB0
[ 333.223335] option 2-3.1:1.0: device disconnected
[ 333.223474] option1 ttyUSB1: GSM modem (1-port) converter now disconnected from ttyUSB1
[ 333.223500] option 2-3.1:1.1: device disconnected
[ 333.224240] option1 ttyUSB2: usb_wwan_indat_callback: resubmit read urb failed. (-2)
[ 333.224424] option1 ttyUSB2: usb_wwan_indat_callback: resubmit read urb failed. (-2)
[ 333.224569] option1 ttyUSB2: usb_wwan_indat_callback: resubmit read urb failed. (-2)
[ 333.227969] option1 ttyUSB2: GSM modem (1-port) converter now disconnected from ttyUSB2
[ 333.228023] option 2-3.1:1.2: device disconnected
[ 333.228874] option1 ttyUSB3: usb_wwan_indat_callback: resubmit read urb failed. (-2)
[ 333.229044] option1 ttyUSB3: usb_wwan_indat_callback: resubmit read urb failed. (-2)
[ 333.229199] option1 ttyUSB3: usb_wwan_indat_callback: resubmit read urb failed. (-2)
[ 333.230722] option1 ttyUSB3: GSM modem (1-port) converter now disconnected from ttyUSB3
[ 333.230750] option 2-3.1:1.3: device disconnected
[ 333.231916] usb 2-3.1: Disable of device-initiated U1 failed.
[ 333.233203] usb 2-3.1: Disable of device-initiated U2 failed.
[ 333.234481] cdc_mbim 2-3.1:1.4 wwan0: unregister 'cdc_mbim' usb-3610000.xhci-3.1, CDC MBIM
[ 333.305762] usb 2-3.1: Set SEL for device-initiated U1 failed.
[ 333.307035] usb 2-3.1: Set SEL for device-initiated U2 failed.
[ 333.634823] usb 2-3.1: reset SuperSpeed USB device number 3 using tegra-xusb
[ 333.661288] option 2-3.1:1.0: GSM modem (1-port) converter detected
[ 333.661547] usb 2-3.1: GSM modem (1-port) converter now attached to ttyUSB0
[ 333.661609] option 2-3.1:1.1: GSM modem (1-port) converter detected
[ 333.661866] usb 2-3.1: GSM modem (1-port) converter now attached to ttyUSB1
[ 333.661916] option 2-3.1:1.2: GSM modem (1-port) converter detected
[ 333.663357] usb 2-3.1: GSM modem (1-port) converter now attached to ttyUSB2
[ 333.663427] option 2-3.1:1.3: GSM modem (1-port) converter detected
[ 333.663620] usb 2-3.1: GSM modem (1-port) converter now attached to ttyUSB3
[ 333.687379] cdc_mbim 2-3.1:1.4: cdc-wdm0: USB WDM device
[ 333.688313] cdc_mbim 2-3.1:1.4 wwan0: register 'cdc_mbim' at usb-3610000.xhci-3.1, CDC MBIM, 6e:6b:e2:fc:58:16