Part Number: DP83867E
Good afternoon,
I have a board with 5 ethernet interfaces with DP83867E is used as PHY.
3 out of 5 ethernet interfaces are up and running but 2 of them are not working.
When I check data length matching (clk, 4 data and ctrl) I see there is a 335 mil difference from max and minimum at transmit path of PHY.
There is 145 mil difference in the receive path of the PHY.
These are not according to your snla387 design layout checklist.
But one of the working interface, I also see a 1 inch of delta in TX signal group.
Could you please inform me more about why we have these hard requirements on your application report (snla387)?
Best regards,
Onur Kusakoglu