Part Number: TCAN1146-Q1
Dear team,
The test condition is that KL30 is always on(12V battery), KL15 is disconnected. After KL15 is turned off completely, they use CANoe sends CANFD frame(CANID: 0x400, baud rate is 500k+2M, data is all zero), but the INH pin is always ~0.44V. Under the same condition, if they sends CAN frame, INH pin will rise to 12V.
Therefore we want to know whether our device support such normal CANFD frame wakeup. If so, could you please help analyze why the customer failed the test? Thanks!
Thanks & Best Regards,
Sherry