This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TG720S-Q1: 100BASE-TI and 1000BASE-T1

Guru 11500 points
Part Number: DP83TG720S-Q1


Hello,

My customer is considering using the DP83TG720S-Q1 for an automotive application.

Is it possible to use the DP83TG720S-Q1 to support 100BASE-T1 and 1000BASE-T1 according to the user's settings?

Thank you.

JH

  • Hi JH,

    TI doesn't have automotive ethernet PHYs which support dual speed (100M and 1000M).

    However, the automotive ethernet PHYs TI develops are pin-2-pin compatible.
    We can leverage this to make a common design/layout for both 100M and 1000M applications. You can use DP83TG720 for 1000Base-T1 and DP83TC812 for 100Base-T1. Switch over between these both parts can be done with few BOM changes.
    We can support you with relevant hardware rollover guides for your design.

    Please let me know if you need more details.

    --
    Regards,
    Gokul.