Part Number: DS90UB953A-Q1
Hi Team,
I have a question about 953 PatGen total line per frame.
Default value of total line per frame (Reg 0x0A, 0X0B) is 0x20D (525), active line per frame (Reg 0x08,0x09) is 0x1E0 (480), front porch (Reg 0x0F) is 0x0A (10), back porch (Reg 0x0E) is 0x21 (33). So Vtotal (525) is not equal to 480+10+33 = 523. Is it an error? Or when I do the calculation, I need to add 2 extra lines?
Thanks,
Ying