This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC812R-Q1: DP83TC812R SQI Monitoring

Part Number: DP83TC812R-Q1


HI

I am using the following to monitor the SQI values for DP83TC812R-Q1 PHY

Read from extended register 0x871 bus , I read the SQI value as 0x7

But the SQI value  is not consistent if I unplug/plug the cables, the SQI changes from 0 and stays at 0 instead of changing to 0x7, are there any steps I am missing

Is my test procedure correct ? or i am missing any steps ?

Example: to read register 0x17 in MMD1F field with no post increment
Step 1) write 0x1F to register 0xD

Step 2) write 0x871 to register 0xE

Step 3) write 0x401F to register 0xD

Step 4) read register 0xE

Regards

Annamalai