Part Number: SN75DP126
Hi,
A customer to us uses Video Mux, SN75DP126SSRHUR, to distribute DP++ to DVI-I. When this is done, we face an radiated EMC issue at the clock frequency of 148.3MHz. We have found a couple of configuration parameter that have an impact on these TMDS signals, one of them is the VSADJ, which according to the datasheet recommends a resistor value of 4.7kohm ±1kohm, see below. However, we see that a further increase to 10kohm reduces the signals amplitude further, is it okay to use resistor value outside 4.7kohm ±1kohm?
HDMI/DVI Sink Differential Voltage Swing Control. An external resistor connecting this pin to GND determines the output voltage swing. A value of 4.7 kΩ is recommended to provide a typical swing of 1000 mV. VSadj resistor values of 4.7 kΩ ± 1 kΩ control the output voltage swing in a near-linear function of approximately 2 VSadj 56 mV/100 Ω.
Further more, we see that also enabling the Pre-emphasis by pulling SDA_CTL/PRE high, have impact on the signal strength. Is there any other parameter we could configure to improve EMC radiated issues with?
Our customer have common-mode choke on the TMDS output signals, is this recommended or do you have any other preferred suggestion to improve radiated emission?
Thanks in advance.
BR
Jörgen Eriksson