Part Number: DS90UB935-Q1
Hi Team,
If a 23.375MHz Ref clock is used on the deserializer side in synchronous mode, but 25MHz is needed as the clock out to the imager, would the following be the best PLL settings for Clock Out accuracy and minimal Jitter?
Ref Clk = 23.375MHz
FC = 160
FC Data Rate 4.16Gbps
HS_CLK_DIV = 4
M = 5
N = 187
Clk Out = 25MHz
Calculated Jitter would be 1.069 ns and a Clock out error of 0%.
Is my understanding and calculations correct. Are there any better settings for lower jitter/error?
Thanks,
Justin