Other Parts Discussed in Thread: USB2ANY
Could you let us know the purpose and the detailed operations of the MCU (AT90USB1286t) on the evaluation board?
Do you have the code for the MCU?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you let us know the purpose and the detailed operations of the MCU (AT90USB1286t) on the evaluation board?
Do you have the code for the MCU?
Thanks.
Hi Child,
In the past, we had used the MCU for configuring the retimer. We have now shifted to using a USB2ANY device to interface the GUI with the DS125DF410.
Thanks,
Drew
Drew,
Any more details that you can release? The MCU seems to be doing something in the background. For example, all the Lock/Sig Det LEDs are controlled by the MCU based on the schematics. Is the MCU "secretly" and autonomously communicating with DS125DF410 during normal operation? How can we stop it from doing anything in the background? We don't want it to affect the I2C communication between our external CPU board and the DS125DF410 chip.
Thanks.
Child
Hi Child,
I think the MCU may do some additional polling in order to control the LEDs. I think there are a couple things you could look at if you're concerned about the I2C communication.
1) Use a logic analyzer to monitor the I2C lines in order to determine specifically what impact the MCU may have.
2) Remove the 0 Ohm resistors connecting the MCU to the SDA/SCL lines in order to ensure that it does not interfere. If there is additional concern about the impact that the MCU has on other pins, consider removing the MCU.
Thanks,
Drew