Part Number: DS125DF410
We inspected the exported data from SigCon of the following eye diagram:

We noticed that the horizontal data length of the exported data is 128, twice the normal length of 64. It seems to us that SigCon just concatenates two identical sets of data to form the eye diagram. Our question is: How can we be sure that the original set of data of horizontal length of 64 represents 100% of the UI ?
In addition, is there a way to adjust the phase so that the eye can be centered in the original data set?
Thanks.
Child