Part Number: DS90UB954-Q1
Hi Team,
We are using a combination of 933 and 954 and connecting them with an STP cable.
Please tell me about the forward channel transfer rate of FPD-LINK III.
First question.
Is the forward channel transfer rate fixed at 4.16Gbps (fFC = 2.1GHz) per channel?
Second question.
The image data sent from 933 is 1.063 Gbps.
(Details)
YUV422 8 bits, so RAW10
fPCLK is 66MHz
Formula = fPCLK/2*28*15% overhead
=66/2*28*1.15 = 1.0626Gbps
Am I correct in understanding that at this time, we are using only 1.063 Gbps for a bandwidth of 4.16 Gbps, so the utilization would be about 25.6%?
The back channel is omitted.
Third question.
Is the bandwidth (3.097Gbps) that does not contain data (3.097Gbps) filled with dummy data, etc.?
(3.097Gbps = 4.16Gbps - 1.063Gbps)
Best Regards,