Please suggest the suitable part for below combination, for bandwidth calculation consider 2MP 60FPS and capable to drive up to 10 meters coxial cable.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please suggest the suitable part for below combination, for bandwidth calculation consider 2MP 60FPS and capable to drive up to 10 meters coxial cable.

Hello Ajay,
can you please provide the Data Type (or # of bits/pixel) as well, since this is a very important factor to calculate the correct Datarate.
Hi Ajay,
may be I was not clear enough. You have 3 options; 1 with CSI-2 in CSI-2 out, the other with CSI-2 in DVP out and the third with DVP in DVP put. So, I am looking for the data type generated by the image sensors and fed to the Serializer in all three cases.
One info upfront, with the DVP options you can't support 2MP camera with 60 FPS