Part Number: DS100DF410
Other Parts Discussed in Thread: DS110DF410, DS250DF410
Dear team,
Hope you are doing well!
Recently, my customer chose to use DS100DF410.
However, they found that the DS100DF410 interface may go up-down, which means that the DS100DF410 will have a short discontinuous or interruption during data transmission when the temperature have a quick change from -20℃ to 75℃(10℃ changing per minute, and the DS100DF410 works normal under the continuous high or low temperature status).
Have you ever met this kind of problem?
If so, how can we solve this problem? Can it be solved by setting the parameters for this temperatures changing quickly circumstance?
Really appreciate your help and support!
I'm looking forward to your reply.
Best regards,
Xenon Li