Part Number: DP83TD510E
Hello,
the figure 6-1 in the datasheet shows the power up diagram. Is this optional or mandatory.
Questions:
- is the clock XI needed in the power up phase?
- they want to use the clock generated by the MCU and so it is a little delayed
- does the reset have to be low during powering up?
- do you have MCU example code or an app note?
- is there any speciality on the Internalisation where the MCU has to care for?
Regards, Holger