Part Number: DS90UB960-Q1
Dear,
It's our block diagram.

In normal case, the DS90UB960 work.
I means that If we use the camera's defined image size, it's work.
( defined image size >> effective image size H:1280 V:720 )
output image height H: 3300 V:750
But, In abnormal case the DS90UB960 doesn't work.
I means that If we use the camera's user defined image size, it doesn't work.
( user defined image size >> effectiv image size H:1024 V:768 )
output image height H:0 V:0
Please, let me know if there is a way to recognize the image even this case ? ( abnormal case )
best regards,
hosung shin.