This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does TI have inverter solution for the hydrogen electrolyser?

 Hi,

Can i check if TI has any industrial controller design and inverter for the hydrogen electrolyser.

The range of the inverter operation is :

DC voltage is around 30 V, and DC current is around 100 A. Yet to test out to finalise these numbers. The out current need to be controllable.

The controller will vary the current depending on the

  • hydrogen output requirements
  • Cell temperature
  • Flow rate control

Best regards,

Felix