Part Number: DS90LV031A
I received a batch of PCBs that use the DS90LV031ATMTC/NOPB (Quad LVDS drivers). The parts are consuming ~400mA at 3.3V when receiving 100Mbps PRBS, which is more than x10 my expectation. Their free air temperature is reaching ~90C. The PRBS pattern does seem to get reliability transmitted through the chip.
I'd like to verify that these chips are genuine, not counterfeit. A graphic with the part markings are attached. They read:
9BALH6U
DS90LV
031AT
The first line is preceded by the National Semiconductor symbol.
Does anyone have a way to help me know if this part is legit?
Thanks,
Tyler