Other Parts Discussed in Thread: SN65HVD10, SN55LBC172, SN65HVD1787, SN65HVD1793
I recently redesign a circuit board for obsolescence and among other things replaced the RS-485 drivers and receivers with a transceiver. The previous design used SN55LBC172 drivers, the new design uses SN65HVD10. During a critical design review our customer informed us that they sometimes use the hardware in a configuration that is not compliant with the EIA-485 specification (I waiting to get specifics on this environment but I know it has to do with cable length) but that original hardware worked ok in this non-compliant configuration. They are concerned that there is risk that the driver in the new transceiver will not necessarily work in this non-compliant configuration. We are just starting to build prototype hardware for the redesign and are looking to determine if this new transceiver will work.
I know this is a long shot but I am wondering:
Are both parts fabricated with the same process?
If so are the output buffer designs in the two parts the same?
I know they are different voltages but since these are differential outputs I don't know if that necessarily means they are different designs.
Thanks,
Barry