Part Number: MAX232
Hi,
What will be the maximum baud rate that can be operated using the MAX232IDR ??. In the datasheet, it is given that the max. speed is 120kbps. In terms of the baud rate, what will be the max. baud rate, which can be used for this module?