Part Number: DS90UB953A-Q1
Hi,
I'm using the DS90UB953A.
Can it work as I2C slave or it's only I2C master.
BR
Shmuel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953A-Q1
Hi,
I'm using the DS90UB953A.
Can it work as I2C slave or it's only I2C master.
BR
Shmuel
Hello Shmuel,
This depends on your use case. If your I2C Master is connected at the DES side and you are communicating with the SER over the Back Channel and using this communication to communicate and configure the other slaves on the SER side, then the SER always works as Master in this case. If you have another Master at the same I2C Bus, then this master must support Multi-Master arbitration.
Hi Hamzeh,
If I'm not working with SER as a back channel, is it works as I2C slave?
BR
Shmurl
Do you mean your I2C Master is attached to the SER? i.e. on the same I2C bus?
In this configuration, the SER acts as a slave on the local I2C bus
Hi,
I mean that I have a controller with master I2C connect to 953.
Can the controller control the 953? Is this connection is valid?
BR
Shmuel
As I said, If the I2C Master is attached to the SER, then the SER acts as a slave on the local I2C bus