Part Number: SN65HVD232
hi, im using SN65HVD232 in my design interfacing with ST32F103C8T6. Some times the ic burns without no reason when connecting to bus. here with i have attached the schematic please check.


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD232
hi, im using SN65HVD232 in my design interfacing with ST32F103C8T6. Some times the ic burns without no reason when connecting to bus. here with i have attached the schematic please check.


Kalisankar,
In addition to Clemens comments, because I agree there should be some protection on the CAN bus, is there anything in particular happening in the application when this damage occurs?
Regards,
Eric Hackett
Hi Eric,
While connecting to the bus, the IC burns and 3.3V and GND lines gets short. once i remove the IC everything works fine.
Kalisankar,
Can you give more details of the application? The CAN IC should not be immediately burning up when it is connected to the bus. It sounds like there is damage occurring to the CANH and/or CANL pins immediately which shorts 3.3V supply pull-up on CANH to the ground connection on CANL.
Regards,
Eric Hackett
Hi Eric,
The application is to monitor the battery and load parameters. The battery BMS and load has termination resistors so i did not add and resistors in CANH and CANL lines. and also there is no Pull-up or Pull down resistors in CAN lines. When i hot plug my devce in the bus between battery and load some times the can IC fails in my circuit only.
Hi Clemens,
Thanks for you advice. Here with i have attached modified PCB layout. Please check and let me know.

Kalisankar,
Have you looked at the signal on CANH and CANL upon insertion/connection? If the different nodes of your device have different ground potential levels, then it could possibly cause a severe voltage differential during connection.
Also, do you know the effective termination strength of the BMS?
Best,
Danny