Part Number: DP83822EVM
Hi,
regarding the idea of using the DP83822, I see that the evm is ready to mount an SFP connector+frame to experiment with the 100base-FX (fiber).
There is a list of components to remove/add, described in the EVM user guide.
But the most impostant point is that the device equipped is the DP83822RHBR (as listed in the BOM): which has no support for the fiber optic interface (only available in -IF or -HF derivatives).
In my opinion also the PHY should be substituted with one of those.
Do you agree?
regards
Alberto