Part Number: TUSB320
I want to verify is this description of EN_N for TUSB320I. “Enable signal; active low. Pulled up to VDD internally to disable the TUSB320 device. If controlled externally, must be held high at least for 50 ms after VDD has reached its valid voltage level.”
So the user has to provide the means to hold EN_N high for 50ms before pulling it low. I am not seeing this implementation shown in the datasheet. Actually, section 8.3 which is the initialization Setup has no mention of it. So the question is this statement valid?