Part Number: TIOS1013
Other Parts Discussed in Thread: TIOS1015, , TIOS101, TIOS102
We are looking to use either the TIOS1013 or TIOS1015 to implement industrial digital outputs.
The TIOS101x devices will be incorporated into an existing hardware design which is powered from a local 3V3 supply and, as such, will be permanently driving the IN and EN pins on the TIOS101x device (either at 0V or 3.3V). However, the TIOS101x device may or may not have power applied to the VCC pin depending upon where the field-side supply is derived from, (i.e. if the field-side supply is derived from an external source this may not be permanently connected until needed), meaning the internal LDO is turned off.
The absolute maximum ratings for the TIOS101x device show digital input min/max limits of -0.3V and 6V. So does this infer that when the TIOS101x part is unpowered it is still acceptable to have a voltage applied to the IN or EN inputs without causing damage to the TIOS101x device or the logic device driving the IN or EN inputs? The absolute ratings do not provide a limiting maximum current in to or out of the digital input pins which is what I would normally expect if the inputs were diode clamped to the VCC OUT supply.
Secondly, the datasheet states that the VIL is 0.8V max and VIH is 2.0V min. Is this irrespective of the VCC IN/OUT voltage? Can I use either the TIOS1013 or TIOS1015 but still drive from 3V3 logic?
We could implement the TIOS101 device and connect our 3V3 supply to the VCC IN pin on the device however I'm not sure whether we would have problems when the VCC pin is un-powered. We have also noted that availability of this part isn't good in the short term so I'm trying to design using parts available at this moment of time.
Thanks in advance.