Part Number: DS90UR903Q-Q1
Description of the issue:
We have had several field failures of the serializer (PN: DS90UR903QSQE/NOPB), where the 1.8V power is shorting to 3.3V power inside the chip after failure. When the boards are diagnosed, all devices connected to the serializer are fine, the only device failing is the serializer itself, U34 in the schematic below.
Notes:
- At first, we suspected ESD: But we have applied up to 15KV from an ESD gun to all external pins and have damage other parts but we have verified that the ESD high voltage has never propagated through to the serializer.
- Note that the serializer/deserializer pair below are used to cross an isolation barrier via the use of transformers.
- Note that the deserializer, U32 is operating with exactly the same power rails and control signals, yet we have never seen it fail.
- Note that the 1.8V and 3.3V power supplies (schem below) are not sequenced and simply come up based on the regulators feeding them, both regulators are fed by a 5V regulator. Do you think that having the 1.8V come up prior to the 3.3V could cause the above mentioned failure i.e., 1.8V shorted internally to 3.3V?
- Have you seen this failure before?
Thanks,
Oliver