This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401A: HDMI diff pairs series capacitors

Part Number: TFP401A
Other Parts Discussed in Thread: DM388

Hi,
We are developing a device with 1920x1080 60Hz LCD panel and TMS320DM388 processor now.

Type-C connectors and USB cable is used for transfer HDMI signals from processor’s board to LCD panel's board. I have a question about AC-couple capacitors on high speed TMDS differential pairs (3xData and 1xClock). Did I should to set 0,1uF capacitors on high speed lines? Did I should place capacitors on host o device side if needed? I use ESD protection IC (TPD12S016PW) on host and slave sides and ferrite differential filters DLP11SA900HL2B on both side now. Is this approach is correct?
Regards, Maxim