Part Number: DS90UB934-Q1
In the development of the mass production project of the rearview mirror in streaming media, DS90UB934 is used to unstring. At present, in the product development, it is found that the output signal of the unstring will occasionally lose 36 lines of data.
As follows:
934 in normal use on the left, the line signal in the red circle is available, and the line signal in the red circle is not available for the abnormal one on the right.
Normal conditions:
Output V total 420, abnormal case, output V total 384
PIN10 Normal no normal.