Part Number: TLK110
Hi,
I try to do a 10BASE-T compliance test on our hardware with a TLK110. So far, "10BASE-T Link Test Pulse" compliance test was successfull.
Now I want that TLK110 transmits a "TL_IDL" signal. Therefore I have set the register of the TLK110 as mentioned in the snla266 document:
1. Register 0x1F set to 0x8000
2. Register 0x00 set to 0x0100
3. Register 0x19 set to 0x0021
4. Register 0x16 set to 0x7108
5. Register 0x1F set to 0x4000
I can not see any frames transmitting. Only link pulse is generated by the TLK110.
I have also tried to have a link partner on the receive lane that generates link pulses (test fixture is not connected). But TLK110 still sending out link pulses only.
Any idea what I'm doing wrong?
Thanks and best regards,
Patrick