Part Number: TUSB4041PAPEVM
Hello,
I'm using the TUSB4041PAPEVM evaluation board together with "TUSB80xx_EEPROM_Programmer_V1.0.0.1" toolkit
The EEPROM was empty (0xFF) from delivery and I have know made my unique configuration file to load into EEPROM
By entering value 0x55 at address 0x00 the device should read configuration from external EEPROM
Switches are set accordingly,
| SW1-2 | SMBUSz | PU : 1 = I2C mode, 0 = SMBus mode | PU 1kohm | OFF -> PU | |
| SW1-3 | SCL | PD : I2C serial clock | PU 1kohm | ON -> PU | |
| SW1-4 | SDA | PD : I2C serial data | PU 1kohm | ON -> PU |
The "on-time program" of EEPROM works as expected, but now there is no access to the EEPROM from the toolkit SW anymore ...

How to resolve this issue ?
Regards,
Ola